This article applies to the Axis I8116-E Network Video Intercom using firmware 11.8.66. ExacqVision does not currently support SIP calling functions. However, this device can be integrated for interactive operation with ExacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the door station call button brings… Continue reading Using the Axis I8116-E Network Video Intercom with ExacqVision
Tag: Access Control
Using the Axis A8207 Door Station with exacqVision
This article applies to the Axis A8207-VE and A8207-VE MkII Network Video Door Stations using firmware 11.5.64. exacqVision does not currently support SIP calling functions. However, these door stations can be integrated for interactive operation with exacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the… Continue reading Using the Axis A8207 Door Station with exacqVision
Adding a Kantech KT-1 with ioSmart Reader to Cloudvue
This video will walk you through connecting a Kantech KT-1 controller using an ioSmart Reader to Cloudvue. Be sure you have followed the steps in a separate video on configuring the KT-1 Controller for Cloudvue Mode before proceeding. <br>
Kantech ioSmart Reader Firmware Update Tool
This video walks users through the process of updating the firmware of ioSmart Readers using the ioSmart Reader Firmware Update Tool over an RS-485 connection. <br>
Incorrect Data Centre Registering KT-1 to Cloudvue
Description When converting a KT-1 to Cloudvue mode sometimes the datacenter does not save to the correct location. Product Steps to Reproduce Expected Results Data centre is saved as EMEA or AU Actual Results Data centre still says North America and it is not on any data centre Solution Ensure the KT-1 is on FW… Continue reading Incorrect Data Centre Registering KT-1 to Cloudvue
KT-1 Controller with ioSmart Reader Wiring
This video shows example diagrams on wiring a Kantech ioSmart reader to the KT-1 and KT-1 PCB single-door controllers. The diagrams displayed in the video can also be viewed below. <br>
ioSmart Mobile Access Control Feature Sheet
Cloudvue Access Control Credentials
Learn how to add Credentials to your Cloudvue hosted access control devices to permit them to enter using your installed readers.
Installing Cloudvue Access App
Description Instructions for installing the Cloudvue Access app for both Android and Apple devices. Product Solution Android iOS Verify The Device Once Installed you must first verify your mobile device before being able to control devices
KT-1 Controller Firmware v3.09.xx Required For Cloudvue Mode
Description In addition to requiring a network with internet access the Kantech KT-1 controller must be running firmware v3.09.xx in order to run in Cloudvue Mode. Solution To determine the current firmware version, access the KT-1 controller from a web browser. Type https:// and the IPv4 address of the KT-1 or if using the MAC… Continue reading KT-1 Controller Firmware v3.09.xx Required For Cloudvue Mode