Failing email notifications after update to Enterprise Manager version 23.09.9.0

April 4th, 2024 Enterprise Manager may fail to send email notifications after update to 23.09.9.0. ExacqVision support has identified an issue with failing email notifications after updating Enterprise Manager from a previous version to version 23.09.9.0 and up. This occurs when checking “Anonymous” as the send user, or additional configuration required for Exchange servers has… Continue reading Failing email notifications after update to Enterprise Manager version 23.09.9.0

Can’t reinstall the EM server

When uninstalling Exacq EM server version 23.06 or above and reinstalling it again on the Windows unit, It will not complete the installation and ask to close the open session even if no sessions are open. Root cause The root cause of this issue is The Microsoft Open Database Connectivity (ODBC) that was not removed… Continue reading Can’t reinstall the EM server

Recording Not Possible – Windows DST Issue

Description  If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST).  Use the following instructions to verify and resolve the issue.  Product  Solution These instruction are based on Windows… Continue reading Recording Not Possible – Windows DST Issue