Unable to Install Exacq Edge on Illustra Camera FW 25.09

Description A new cybersecurity cipher introduced is not yet included in the current exacqEdge installer for Illustra cameras. As a result, exacqEdge installation or upgrade may fail on affected devices.Engineering is actively working on an updated installer that will support this new cipher in a future release. Product Issue Illustra cameras running firmware 25.09 may… Continue reading Unable to Install Exacq Edge on Illustra Camera FW 25.09

Installing Exacq Edge 25.01 on Illustra Camera with FW 25.09

Warning: Level 3 Document – Please do not distribute.   Description This article documents the correct procedure for installing Exacq Edge 25.01 on cameras that are currently running firmware 25.09, which blocks installation of Exacq Edge due to cipher restrictions. Product Steps to Reproduce Expected Results Exacq Edge 25.01 installs successfully. Actual Results A pop‑up… Continue reading Installing Exacq Edge 25.01 on Illustra Camera with FW 25.09

ExacqVision Edge v26.0.1.0

H1 2026-02-10 ev-Server-axis-armhf^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_armhf.eap^13 February 2026^14.5MB, H1 2026-02-10 ev-Server-illustra-aarch64^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_illustra-aarch64.tar^13 February 2026^21.4MB, H1 2026-02-10 ev-Server-ARTPEC8^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_ARTPEC-8.eap^13 February 2026^21.5MB, H1 2026-02-10 ev-Server-ARTPEC8-OS12^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_ARTPEC-8_OS12.eap^13 February 2026^21.5MB, H1 2026-02-10 ev-Server-axis-arm^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_AxisArm.eap^13 February 2026^14.4MB, H1 2026-02-10 ev-Server-ARTPEC4^Version 26.0.1.0^https://cdnpublic.exacq.com/26.0/exacqVisionServer_26.0.1.0_ARTPEC-4.eap^13 February 2026^14.9MB,

Edge Server Application Stops Shortly After Starting on Illustra Cameras

Description Users setting up the ExacqVision Edge or Edge+ application on Illustra cameras may see the application running and connect to it only to find it stops running shortly thereafter. This is likely due to changing the default ‘Enable Event Record’ setting on the camera. <br> Product Cameras: Edge Server <br> Steps to Reproduce <br>… Continue reading Edge Server Application Stops Shortly After Starting on Illustra Cameras

PortCheck Utility

When troubleshooting TCP/IP connectivity issues, it is often helpful to confirm that the network path is open over a specified port and that there is no interference from a firewall or antivirus. This also rules out software level problems that may be causing a failure to connect. While there exists many utilities to accomplish this… Continue reading PortCheck Utility

ExacqVision Edge Legacy Versions

{2024} Q4 2025-02-20 ev-Server-axis-armhf^Version 24.12.7.0^https://cdnpublic.exacq.com/24.12/exacqVisionServer_24.12.7.0_armhf.eap^20 February 2025^7.2MB, Q4 2025-02-20 ev-Server-illustra-aarch64^Version 24.12.7.0^https://cdnpublic.exacq.com/24.12/exacqVisionServer_24.12.7.0_illustra-aarch64.tar^20 February 2025^9.6MB, Q4 2025-02-20 ev-Server-ARTPEC8^Version 24.12.7.0^https://cdnpublic.exacq.com/24.12/exacqVisionServer_24.12.7.0_ARTPEC-8.eap^20 February 2025^9.7MB, Q4 2025-02-20 ev-Server-axis-arm^Version 24.12.7.0^https://cdnpublic.exacq.com/24.12/exacqVisionServer_24.12.7.0_AxisArm.eap^20 February 2025^7.2MB, Q4 2025-02-20 ev-Server-ARTPEC4^Version 24.12.7.0^https://cdnpublic.exacq.com/24.12/exacqVisionServer_24.12.7.0_ARTPEC-4.eap^20 February 2025^8.0MB, Q3 2024-09-19 ev-Server-axis-armhf^Version 24.09.5.0^https://cdnpublic.exacq.com/24.09/exacqVisionServer_24.09.5.0_armhf.eap^21 October 2024^7.2MB, Q3 2024-09-19 ev-Server-illustra-aarch64^Version 24.09.5.0^https://cdnpublic.exacq.com/24.09/exacqVisionServer_24.09.5.0_illustra-aarch64.tar^21 October 2024^9.6MB, Q3 2024-09-19 ev-Server-ARTPEC8^Version 24.09.5.0^https://cdnpublic.exacq.com/24.09/exacqVisionServer_24.09.5.0_ARTPEC-8.eap^21 October 2024^9.7MB, Q3 2024-09-19 ev-Server-axis-arm^Version 24.09.5.0^https://cdnpublic.exacq.com/24.09/exacqVisionServer_24.09.5.0_AxisArm.eap^21 October 2024^7.2MB,… Continue reading ExacqVision Edge Legacy Versions