Category: exacqVision Integrations Other
Illustra Flex4 Indoor PTZ with bubble
Description Illustra Flex4 Indoor PTZ with bubble showing distorated images on zoom. Product Illustra Flex 4 PTZ all firmware Steps to Reproduce Turn off the Tilt Limit in the camera PTZ settings Expected Results Camera zoom shows in focus and sharp Actual Results Camera zoom is slightly disorted and out of focus Solution This is… Continue reading Illustra Flex4 Indoor PTZ with bubble
Exacq I/O USB module Output Mapping in Exacq
Description This document will outline the mapping of the USB I/O module for the output alams in exacq Product Exacq Server Exacq Integrations Output 1 – Relay ( 1 on image )Output 2 – Output 1 ( 2 on image )Output 3 – Output 2 ( 3 on image )Output 4 – Output 3 (… Continue reading Exacq I/O USB module Output Mapping in Exacq
Road AI LPR application with Hanwha Cameras
Overview Hanwha cameras may be configured with the Road AI license plate recognition application. The data from license plate captures can be viewed in the ExacqVision Client as text, sent as serial data over IP. The Road AI application is pre-installed and licensed from the factory on select camera models. This document will step through… Continue reading Road AI LPR application with Hanwha Cameras