Configuring exacqVision With Your Identity Provider (IdP) 1. Introduction exacqVision now supports modern authentication standards through OAuth 2.0 and OpenID Connect (OIDC), enabling secure user authentication through popular identity providers such as Okta and Microsoft Entra ID (Azure AD). This guide walks through: 2. OAuth and OIDC Basics (Vendor‑Agnostic) OAuth 2.0 and OpenID… Continue reading exacqVision OAuth Integration Guide
Category: exacqVision Integrations
Illustra Encoder FPS Options Not Fully Displayed in Exacq
Description The Illustra encoder does not display the full list of available FPS values in Exacq.On the encoder’s web interface, the FPS options appear as a continuous range from 1–30 FPS, but Exacq only displays a subset of these values. This has been identified as a camera firmware issue and will be resolved in a… Continue reading Illustra Encoder FPS Options Not Fully Displayed in Exacq
How-To: Configure Exacq Notifications to Microsoft Teams Using Power Automate
Description This document explains how to configure ExacqVision email notifications, event linking, and a Power Automate flow to post alerts into Microsoft Teams. Product – exacqVision software – Microsoft Teams/Outlook/Power Automate Steps to Configure 1. Configure the Exacq Email Notification Profile 1. Go to Setup → Notifications → E-mail Message Profiles. 2. Create a New… Continue reading How-To: Configure Exacq Notifications to Microsoft Teams Using Power Automate
Illustra Encoder and PTZ Camera Integration TAB
How to Update the USB Serial Driver
Description The following are the steps to update the USB Serial Driver 2. Unzip the driver 3. Open Device Manager and Navigate to Other Devices and drop the arrow down to see the USB Serial. 4. Right Click the USB Serial > Update Driver -> Choose the downloaded driver. Select Browse My Computer for Driver… Continue reading How to Update the USB Serial Driver
Configuration Calculator
This tutorial video showcases the new metadata updates on the exacqVision Configuration Calculator.
25.1 exacqVision Integrator Services Portal User Manual
Hanwha TID-600R Intercom with exacqVision 25H1
This feature included in 25H1 allows the user to integrate the Hanwha TID-600R with exacqVision Client.In this example we will step through an example scenario where pressing the call button or using the Touchless call setting on the intercom brings the camera to the attention of the exacqVision operator to trigger a door lock.Chapters:00:00 Intro00:12… Continue reading Hanwha TID-600R Intercom with exacqVision 25H1
Using the Hanwha TID-600R Intercom with exacqVision
This feature included in 25H1 allows the user to integrate the Hanwha TID-600R with exacqVision Client. Exacq are committed to growing our integration offering with video intercom products. With this release, we are announcing the integration with the Hanwha video intercom offering, building upon the support for existing intercoms from Axis and 2N. This contactless… Continue reading Using the Hanwha TID-600R Intercom with exacqVision
Ccure 9000 Door Held Event issue with Exacq 24.06 and earlier
Description When Activating an event for the door held on Ccure, it will not get activated on Exacq side and will not get triggered via event linking. Product Exacq Server and Client versions 24.03 & 24.06 Ccure 9000 & Firmware=”web=7.0.1174.174, app=4.0.0″ Steps to Reproduce Creating the door held event on Ccure side then trying to… Continue reading Ccure 9000 Door Held Event issue with Exacq 24.06 and earlier