Moving Cameras Between Cloudvue Gateways

Description When a camera is added to a Cloudvue Gateway it is assigned to that specific Cloudvue Gateway in our cloud database. Attempts to add the camera to a different Cloudvue Gateway will fail with a message indicating that the camera “Already Exists”. Here are the appropriate steps to follow in the event a camera… Continue reading Moving Cameras Between Cloudvue Gateways

Cloudvue Advance Replacement RMA Process – North America

Description  Please use the following steps when creating a Cloudvue Advance Replacement RMA in North America. Solution Complete the normal Cloudvue RMA Process for North America, see KB #13217 for instructions. From the RMA Salesforce Case Email Will Anderson <will.anderson@jci.com>  requesting that he create a sales order.  The email should include the following information: IMPORTANT: … Continue reading Cloudvue Advance Replacement RMA Process – North America

Cloudvue NVR Recorder Debugging

Description  At times it can be useful to get nvr-recorder debug level output to troubleshoot recording issue on a Cloudvue Gateway.  This can be achieved using the smv-record debug engine. Product  Solution The basic steps are: Example Tech Tip:  Support Diagnostics also captures this information in the Smartvue-smv-record.log section.

Prompted to “Checkout” When Saving Cloudvue Subscriptions

Description  When using a global admin staff account I am being prompted to CHECKOUT and provide credit card information when updating camera subscriptions. Product  Steps to Reproduce  Expected Results  Actual Results  Solution Check the Partners FIN Type. If the partners FIN Type is set to Stripe then the end user will need to use Cloudvue.com… Continue reading Prompted to “Checkout” When Saving Cloudvue Subscriptions

Setting Cloudvue Engineering Environments

Description The following instructions discuss setting up Cloudvue video devices for use in specific engineering and production environments. Product Cloudvue Gateways The basic steps to specify the use of a particular environment are: Drop and Create smartvuedb Set the Environment Edit the file /smartvue/cloud-config.json to set the desired environment. Development Production Staging Restart nvr-cloud-messaging service… Continue reading Setting Cloudvue Engineering Environments

Unable to Remove Cloudvue Custom View User

Description Custom view users cannot be removed from a view as the checkbox for their user name will be dimmed and cannot be unchecked to deselect the user. Product Solution The user who initially creates a custom view becomes the owner of the view i.e., “Custom View owner” and cannot be removed from the view… Continue reading Unable to Remove Cloudvue Custom View User