CV OnSite Troubleshooting

 Description  This article outlines the steps to troubleshoot situations where the CloudVue device cannot be seen on CV manager. The procedure covers verifying the NVR’s local output, checking for errors at the OS level, and confirming that the required network and internet access are available.  Troubleshooting Steps  1. Check Local Access on the NVR  If you are unable… Continue reading CV OnSite Troubleshooting

CV Port Tester Tool 

Description  The CloudVue Port Tester Tool is used to verify that all required ports and URLs are open for proper connectivity to CloudVue. If any required ports are blocked, the NVR may be unable to establish a connection.  Steps to Use the CV Port Tester Tool  Expected Results  A successful test will display results similar to the following:  If any… Continue reading CV Port Tester Tool 

Missing Cloudvue Data Centers

Description When converting an Illustra camera to Cloudvue mode no Data Center entries appear in the dropdown menu. Product Steps to Reproduce Expected Results Actual Results Solution Reason #1 If the camera firmware is the cause then try using new camera firmware or if one is not available downgrading it to an earlier version. See related… Continue reading Missing Cloudvue Data Centers

Reboot Schedule For Illustra Essentials C2C Removed

Description As a result of Cron being unavailable on Illustra Essential cameras the reboot schedule is unavailable on these devices. Cloudvue Software versions prior to 24.12.x Incorrectly display the reboot schedule. Beginning with the release of Cloudvue Software version 24.12.x the reboot schedule will no longer be displayed. Product Steps to Reproduce Results Prior to… Continue reading Reboot Schedule For Illustra Essentials C2C Removed

llustra Flex2 4k Bullets / Domes Not Recording

Description  If Cloudvue C2C Illustra Flex2 4k Bullet or Dome camera is not recording locally or to the cloud it may be a camera firmware issue. Product  Solution When issue was observed cameras were running the latest production firmware Illustra.SS004.01.09.05.0008 (Flex Gen2), live view was working normally however the cameras were not recording either to… Continue reading llustra Flex2 4k Bullets / Domes Not Recording

Cloudvue Advance Replacement RMA Process – North America

Description  Please use the following steps when creating a Cloudvue Advance Replacement RMA in North America. Solution Complete the normal Cloudvue RMA Process for North America, see KB #13217 for instructions. From the RMA Salesforce Case Email Will Anderson <will.anderson@jci.com>  requesting that he create a sales order.  The email should include the following information: IMPORTANT: … Continue reading Cloudvue Advance Replacement RMA Process – North America

Prompted to “Checkout” When Saving Cloudvue Subscriptions

Description  When using a global admin staff account I am being prompted to CHECKOUT and provide credit card information when updating camera subscriptions. Product  Steps to Reproduce  Expected Results  Actual Results  Solution Check the Partners FIN Type. If the partners FIN Type is set to Stripe then the end user will need to use Cloudvue.com… Continue reading Prompted to “Checkout” When Saving Cloudvue Subscriptions

Setting Cloudvue Engineering Environments

Description The following instructions discuss setting up Cloudvue video devices for use in specific engineering and production environments. Product Cloudvue Gateways The basic steps to specify the use of a particular environment are: Drop and Create smartvuedb Set the Environment Edit the file /smartvue/cloud-config.json to set the desired environment. Development Production Staging Restart nvr-cloud-messaging service… Continue reading Setting Cloudvue Engineering Environments

Illustra Firmware Version SS018.24.03.00.0010 Not Supported on C2C

Description It has been discovered that Illustra firmware SS018.24.03.00.0010 is missing key Cloudvue components and is there for NOT supported on C2C devices. The primary indicator is no data centers will be displayed when converting to Cloudvue mode. Products C2C#Illustra#DescriptionTCCF42V032IFS02IFS02-D12-ITA42MP , 2.7-13.5 MFZ , Mini-DomeTCCF44V032IFS04-D12-ITA44MP , 2.7-13.5 MFZ , Mini-DomeTCCF48V032IFS08-D13-ITA48MP , 3.6-11 MFZ , Mini-DomeTCCF42VI032IFS02-D12-OIA42MP… Continue reading Illustra Firmware Version SS018.24.03.00.0010 Not Supported on C2C

Unable to Remove Cloudvue Custom View User

Description Custom view users cannot be removed from a view as the checkbox for their user name will be dimmed and cannot be unchecked to deselect the user. Product Solution The user who initially creates a custom view becomes the owner of the view i.e., “Custom View owner” and cannot be removed from the view… Continue reading Unable to Remove Cloudvue Custom View User