FFNI on stream %1 – %2

FFNI on stream %1 – %2 Description FFNI indicates First Frame Not I-frame. The psfpi plugin cannot start recording on a P/B-frame since these cannot be decoded. The FFNI metrics/logging is accounting for the fact that frames were dropped. Possible symptom is “smearing” of video occasionally “snapping” back to clear image. The stream ID will determine… Continue reading FFNI on stream %1 – %2

remove D:\\YYYY\\MM\\DD\\HH\\XXXX-XXXXXXXX.ps error

remove D:\YYYY\MM\DD\HH\XXXX-XXXXXXXX.ps error Description The Server tried to remove a previously recorded file and could not. Notes This can occur if the file has manually been deleted, or if another software (anti-virus) has currently locked the file. Also, if a hard drive has been remounted as read-only, the file removal will fail.

File ***.ps not found

File ***.ps not found Description Indicates that that the Exacq Server had knew about this file. But when it went to remove this data to make room for new data, it could not find the file in question. Notes This can mean a few things. It can mean that the drive is falling behind, if… Continue reading File ***.ps not found

System %1 could not get record volume

System *** could not get record volume Description %1 = the stream id. %BR% For that particular stream, we could not find a place to record it. Notes We try to have 1 GB of free space free to record to when we open a file. This is the warning we print if we can’t… Continue reading System %1 could not get record volume