Description The Panasonic WV-S8531N fails to detect motion when using H265 option. Product ExacqVision Server Steps to Reproduce Expected Results Motion is detected and video records. Actual Results Motion is not detected and video is not recorded. Solution Updating firmware to S8531_202ES allowed the camera use Motion with H265 format on Server 22.09. AES-146 <br>
Category: PanasonicPI
Error -10057 (RTSP PLAY: Bad \”Range:\” header).
Error -10057 (RTSP PLAY: Bad \”Range:\” header). Description Camera has stopped sending data. Notes Stream Timeout normally precedes this error. Error -10057 (RTSP PLAY: Bad “Range:” header) is the same error as Stream Timeout. This is a different component calling out the same error.