Profile Descriptìon: %1. Notification attempt return code= 26 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 26 means “Read Error” Notes Notifications which include attaching a clip will attempt to create, then read… Continue reading Profile Description: %1. Notification attempt return code= 26
Category: NotifyPI
Profile Description: %1. Notification attempt return code= 67
Profile Descriptìon: %1. Notification attempt return code= 67 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 67 means “Login Denied” Notes Failed logins to SMTP servers can result due to username/password problems, or… Continue reading Profile Description: %1. Notification attempt return code= 67
Profile Description: %1. Notification attempt return code= 7
Profile Descriptìon: %1. Notification attempt return code= 7 Description %1 – This is the name of the Email Message Profile%BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 7 means “Couldn’t Connect” Notes Connection failures to SMTP servers result when the TCP connection to a given… Continue reading Profile Description: %1. Notification attempt return code= 7
Profile Description: %1. Notification attempt return code= 28
Profile Descriptìon: %1. Notification attempt return code= 28 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 28 means “Operation Timeout” Notes Timeouts to SMTP servers can result due to routing problems between the… Continue reading Profile Description: %1. Notification attempt return code= 28
Profile Description: %1. Notification attempt return code= 55
Profile description: %1. Notification attempt return code= 55 Description %1 = The name of the Email Message Profile. %BR%This is caused by missing data from compliance with RFC5321. This will cause failure with some SMTP servers, but not others, depending on how they accommodate the message. Notes Option 1: If license subscription allows, update exacqVision… Continue reading Profile Description: %1. Notification attempt return code= 55
Searching for video for id %
Searching for video for id % Description A notification profile has been triggered which included the “Attach Preview” option enabled. Video is being searched to include with the notification. Notes This is a normal message.
Unable to communicate with webserver at address %1. Error message: %2
Unable to communicate with webserver at address %1. Error message: %2 Description %1 = IP address of Web Server. %BR% %2 = Specific error message or number. %BR% The IP address or hostname listed on the Notifications>Web Server tab was not reachable. Notes
Profile Description: %1 , Result: *** DD HH:MM:SS %2 sendEmail.exe[***]: Email was sent successfully!
Profile description: %1 , Result: * DD HH:MM:SS %2 sendEmail.exe[*]: Email was sent successfully! Description %1 = Notification Profile name. %BR% %2 = System name. %BR% The Notification Profile triggered and successfully sent an email. Notes Not a problem, unless this occurs way too often. If so, check the Event Linking “Event Type” which triggers… Continue reading Profile Description: %1 , Result: *** DD HH:MM:SS %2 sendEmail.exe[***]: Email was sent successfully!
Loaded configuration from disk successfully
Loaded configuration from disk successfully Notes This is a normal message.