%1: Context %2. Media open but data timed out. Close and retry

%1: Context %2. Media open but data timed out. Close and retry Description The video stream is still open, but we haven’t received video for 10 seconds. %BR%%BR% %1 – Device IP Address %BR% %2 – Device name Notes Will usually be noted just prior to a stream closing due to some sort of loss… Continue reading %1: Context %2. Media open but data timed out. Close and retry

The processing loop has taken too long *** times. The longest time was ***ms for *** passes.

The processing loop has taken too long *** times. The longest time was ***ms for *** passes. Description A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate… Continue reading The processing loop has taken too long *** times. The longest time was ***ms for *** passes.

The processing loop performed *** passes and took ***ms to process the data.

The processing loop performed *** passes and took ***ms to process the data. Description A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate that the CPU is… Continue reading The processing loop performed *** passes and took ***ms to process the data.