Invalid event database – ***

Invalid event database – *** Description The EventPI database may be corrupted. The database is located in the Server folder as “eventpi.db”. Notes The database files are located in the Server folder and start with: eventpi.db .Stop the Server service, delete the files and restart to recreate the database.

Opening|creating database in location: C:/Program Files/exacqVision/Server/eventpi.db

Opening|creating database in location: C:/Program Files/exacqVision/Server/eventpi.db Description In Linux, this will say: /usr/local/exacq/Server/eventpi.db Notes This is a normal message during startup. If the file gets “created” on an existing installation, this indicates there was a corruption or missing database.