FFNI on stream %1 – %2

FFNI on stream %1 – %2 Description FFNI indicates First Frame Not I-frame. The psfpi plugin cannot start recording on a P/B-frame since these cannot be decoded. The FFNI metrics/logging is accounting for the fact that frames were dropped. Possible symptom is “smearing” of video occasionally “snapping” back to clear image. The stream ID will determine… Continue reading FFNI on stream %1 – %2

The DELETE statement conflicted with the REFERENCE constraint “auditlogger_auditlog_user_id_fbf03342_fk_organization_enterpriseuser_id”. The conflict occurred in database “NA”, table “dbo.auditlogger_auditlog

The DELETE statement conflicted with the REFERENCE constraint “auditlogger_auditlog_user_id_fbf03342_fk_organization_enterpriseuser_id”. The conflict occurred in database “NA”, table “dbo.auditlogger_auditlog Description when the Datarolloff service is failing to start you may see this error or a similar error in the datarolloff log file. There is a foreign key constraint that is failing to delete which in turns stops… Continue reading The DELETE statement conflicted with the REFERENCE constraint “auditlogger_auditlog_user_id_fbf03342_fk_organization_enterpriseuser_id”. The conflict occurred in database “NA”, table “dbo.auditlogger_auditlog

Profile Description: %1. Notification attempt return code= 26

Profile Descriptìon: %1. Notification attempt return code= 26 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 26 means “Read Error” Notes Notifications which include attaching a clip will attempt to create, then read… Continue reading Profile Description: %1. Notification attempt return code= 26

Profile Description: %1. Notification attempt return code= 67

Profile Descriptìon: %1. Notification attempt return code= 67 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 67 means “Login Denied” Notes Failed logins to SMTP servers can result due to username/password problems, or… Continue reading Profile Description: %1. Notification attempt return code= 67

Profile Description: %1. Notification attempt return code= 7

Profile Descriptìon: %1. Notification attempt return code= 7 Description %1 – This is the name of the Email Message Profile%BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 7 means “Couldn’t Connect” Notes Connection failures to SMTP servers result when the TCP connection to a given… Continue reading Profile Description: %1. Notification attempt return code= 7

Profile Description: %1. Notification attempt return code= 28

Profile Descriptìon: %1. Notification attempt return code= 28 Description %1 – This is the name of the Email Message Profile %BR% %BR% Notifications are sent using curl, so the return codes are curl status/error codes. %BR% Curl error 28 means “Operation Timeout” Notes Timeouts to SMTP servers can result due to routing problems between the… Continue reading Profile Description: %1. Notification attempt return code= 28

error 86 (invalid password)

error 86 (invalid password) Description If the main server, you are setting up to connect to an archiving target on a s-series is joined to a domain there is a local group policy that needs to be configured or you will get a disconnected status ad error 86 invalid password in the server logs Notes… Continue reading error 86 (invalid password)

LICENSE: Error loading active – Required MAC address missing.

LICENSE: Error loading active – Required MAC address missing. Description This indicates that the MAC Address registered to the license was not found. Notes See suggestions in KB 12830: https://support.exacq.com/#/knowledge-base/article/12830

Download failed (status 6): curl: (6) Couldn’t resolve host ‘cdnpublic.exacq.com’

Download failed (status 6): curl: (6) Couldn’t resolve host ‘cdnpublic.exacq.com’ Description Can’t update the Exacq edge server because can’t resolve the host ‘cdnpublic.exacq.com’ The DNS was not assigned to the camera Notes After assigning the DNS to the camera it begins to update the SW

Profile Description: %1. Notification attempt return code= 55

Profile description: %1. Notification attempt return code= 55 Description %1 = The name of the Email Message Profile. %BR%This is caused by missing data from compliance with RFC5321. This will cause failure with some SMTP servers, but not others, depending on how they accommodate the message. Notes Option 1: If license subscription allows, update exacqVision… Continue reading Profile Description: %1. Notification attempt return code= 55