psycopg2.errors.ForeignKeyViolation: update or delete on table “organization_enterpriseuser” violates foreign key constraint “auditlogger_auditlog_user_id_%1_fk_organizat” on table “auditlogger_auditlog” Description Reviewing Notes %1 suggest the user id number.%BR%See KB 15724 for resolution.
Category: Verbose
The processing loop has taken too long *** times. The longest time was ***ms for *** passes.
The processing loop has taken too long *** times. The longest time was ***ms for *** passes. Description A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate… Continue reading The processing loop has taken too long *** times. The longest time was ***ms for *** passes.
The processing loop performed *** passes and took ***ms to process the data.
The processing loop performed *** passes and took ***ms to process the data. Description A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate that the CPU is… Continue reading The processing loop performed *** passes and took ***ms to process the data.
Network error 7 from request iAPI/element.cgi?action=explain&group=System&group=Network using scheme https.
Network error 7 from request iAPI/element.cgi?action=explain&group=System&group=Network using scheme https. Description 7 means failed to connect to host or proxy Can’t connect via HTTPS Notes Has to change the connection type to HTTP instead of HTTPS
LDAP: Found keytab with SPN EDVR/%1 so no need to query server.
LDAP: Found keytab with SPN EDVR/%1 so no need to query server. Description %1 – This will likely be the Serial number or the MAC address of the Server.%BR%Directory services found a keytab file containing an SPN so will not query AD for the SPN but use the SPN found in the keytab. Notes Linux… Continue reading LDAP: Found keytab with SPN EDVR/%1 so no need to query server.
Client 10.0.6.77:44976 disconnected.
Client 10.0.6.77:44976 disconnected. Description A Client has unchecked this Server on the “Add Systems” page. Notes This is a normal message.
Made system available as a peer time server.
Made system available as a peer time server. Description The Server successfully enabled the local machine as an NTP server. Notes This is a normal message.
Purging log file YYYYMMDD.txt.
Purging log file YYYYMMDD.txt. Description This means that an old Log File has been deleted. Logs are retained up to the “Maximum Days Storage” setting on the “System Log” page. Notes If the OS drive is dangerously full, you may see many log files purged quickly to try to make space.
DiscoveryInprogress State. Unexpected event. Cable Plugged in on MAC %1
DiscoveryInprogress State. Unexpected event. Cable Plugged in on MAC %1 Description %1 = The MAC address of the Nic.%BR% This means a camera was plugged in to one of the POE ports. Notes This is normal on the Una and M-Series.
Idle State. Cable Plugged out on MAC %1
Idle State. Cable Plugged out on MAC %1 Description %1 = MAC Address This indicates that a camera was disconnected from a POE port. Notes This is normally seen on the Una or M-Series.