2023-06 June Quarterly Release Training

ExacqVision Server Bug Fix – Fixed excessive Archiving status messages (AESW-4989) Bug Fix – Debian installer no longer enabled eventpi by default Bug Fix – Fixed issue capturing all metadata when multiple events are sent as one alarm Bug Fix – Ensure eventpi database is purged after server reboot Bug Fix – Fixed connection status… Continue reading 2023-06 June Quarterly Release Training

Cloudvue 22.9.1 Technical Release Notes

Description  Cloudvue Release 22.9.1 is a defect/fix release Product  Cloudvue Deployed InstanceDateNorth America03/08/2023Australia03/13/2023EMEA03/13/2023 Enhancements/Fixes “Force Certify” buttoned added the Cloudvue Manager (CVM) user Interface when the device is offline. Devices with certificate problems appear as offline. This fix provides the CVM a method to assign a certificate while the device is offline. People/Vehicle detection restored to… Continue reading Cloudvue 22.9.1 Technical Release Notes

2023-03 March Quarterly Release Training

ExacqVision Server Bug Fix – Fixed PTZ preset administration for custom users to create presets for analog cameras (AESW-4357) Bug Fix – Fixed monitoring RAID background tasks, like consistency checks and background initialization (AESW-4387) Bug Fix – Fixed reporting incorrect RAM, was displaying MB instead of GB (AESW-2498) Bug Fix – actipi – Reduce metadata… Continue reading 2023-03 March Quarterly Release Training