Axis Q19 Series Thermal Cameras Integration Guide

Description Axis thermal cameras provide heat-based detection for monitoring property or detecting thermal anomalies which could lead to incidents involving smoke or fire. This guide is intended to introduce the use of these devices with your exacqVision VMS software. Requirements At the time of writing this article, these instructions pertain to the Axis Q19 Series… Continue reading Axis Q19 Series Thermal Cameras Integration Guide

Elgato Stream Deck Integration Guide

Overview When configured properly, exacqVision may be configured to react to Elgato Stream Deck to take actions, such as changing camera views or activating output alarms. This is made possible by exacqVision’s Serial Profile settings combined with Event Monitoring or Event Linking. This guide provides the steps needed to get started, which you may customize… Continue reading Elgato Stream Deck Integration Guide

Axis License Plate Verifier Serial Integration Guide

Overview Axis offers a camera-based License Plate Verifier application for detecting and reading vehicle license plates. The data from the license plate captures may be viewed within the exacqVision Client as text, sent as serial over IP data. This document provides the steps to set up the integration with exacqVision. NOTE: This guide is not… Continue reading Axis License Plate Verifier Serial Integration Guide

Using the Axis TU9001 Control Board with exacqVision

This document will guide you through step-by-step procedures for keyboard use and suggested button mappings. Product The Axis TU9001 Control Board consists of the combination of the TU9002 Joystick and the TU9003 Keypad. IMPORTANT: The TU9002 and TU9003 appear to the operating system as separate devices. As of Client version 24.03 only one Joystick device… Continue reading Using the Axis TU9001 Control Board with exacqVision

Using iDRAC on X-Series NVRs

What is iDRAC? Integrated Dell Remote Access Controller (iDRAC) is a proprietary technology that allows IT administrators to remotely manage and monitor Dell-built servers. This includes software and hardware components. The Exacq X-Series NVRs include iDRAC micro ports on the front of the system and iDRAC network interfaces on the back. The location of these… Continue reading Using iDRAC on X-Series NVRs

exacqVision DSX Integration Guide

Overview DSX is a powerful access control system monitoring application. This integration solely supports PTZ, Live View and Recorded View video and utilizes evAPI. <br> Requirements <br> Installation Before configuring WinDSX for use with the exacqVision System, complete the following steps: <br> Configuration <br> <br> <br> <br> <br> NOTE: If socket errors appear when you… Continue reading exacqVision DSX Integration Guide

TrueVUE Cloud Integration Guide

TrueVUE Cloud Integration Guide <br> Overview TrueVUE Cloud is a cloud-based retail analytic software that integrates with ExacqVision Video Recorders. This integration allows retailers to connect video to loss events. This integration is based on ExacqVision’s webAPI. <br> Requirements <br> Configuration <br> Support SensormaticFor Sales and General Inquiries:+1-800-642-7505 (US)Monday – Friday: 9am – 5pm ETExisting… Continue reading TrueVUE Cloud Integration Guide

Road AI LPR application with Hanwha Cameras

Overview Hanwha cameras may be configured with the Road AI license plate recognition application. The data from license plate captures can be viewed in the ExacqVision Client as text, sent as serial data over IP. The Road AI application is pre-installed and licensed from the factory on select camera models. This document will step through… Continue reading Road AI LPR application with Hanwha Cameras

Using the ADVCPTZKEY1 USB Joystick / Keyboard with exacqVision

This document will guide you through step-by-step procedures for keyboard use and suggested button mappings. Prerequisites For proper operation of the American Dynamics ADVCPTZKEY1 PTZ USB Keyboard, both the exacqVision Client and Server must be on version 22.03 or higher. Product  ADVCPTZKEY1 American Dynamics Surveillance Keyboard <br> Setup <br>