Illustra Flex4 Indoor PTZ with bubble

Description  Illustra Flex4 Indoor PTZ with bubble showing distorated images on zoom. Product  Illustra Flex 4 PTZ all firmware Steps to Reproduce  Turn off the Tilt Limit in the camera PTZ settings Expected Results  Camera zoom shows in focus and sharp Actual Results  Camera zoom is slightly disorted and out of focus Solution This is… Continue reading Illustra Flex4 Indoor PTZ with bubble

Exacq I/O USB module Output Mapping in Exacq

Description This document will outline the mapping of the USB I/O module for the output alams in exacq Product Exacq Server Exacq Integrations Output 1 – Relay ( 1 on image )Output 2 – Output 1 ( 2 on image )Output 3 – Output 2 ( 3 on image )Output 4 – Output 3 (… Continue reading Exacq I/O USB module Output Mapping in Exacq

Cloudvue Access – Allowing Bluetooth permissions

Description When using Cloudvue Access to allow opening of doors in near by the application needs to have permission to use bluetooth Product Cloudvue Access Steps to Reproduce Expected Results You see all doors near by Actual Results No doors are seen in near by but location tab shows all doors Solution You need to… Continue reading Cloudvue Access – Allowing Bluetooth permissions

Changing Kantech Smart Service name breaks Integration

Description  Entrapass integration does not connect to exacqVision. Product  Expected Results  Integration adds successfully and shows connected. Actual Results  Integration shows not connected could not connect contact integration. Solution Ensure the Kantech/Entrapass smart service is named ‘SmartService’ in the Entrapass software

Incorrect Data Centre Registering KT-1 to Cloudvue

Description  When converting a KT-1 to Cloudvue mode sometimes the datacenter does not save to the correct location. Product  Steps to Reproduce  Expected Results  Data centre is saved as EMEA or AU Actual Results  Data centre still says North America and it is not on any data centre Solution Ensure the KT-1 is on FW… Continue reading Incorrect Data Centre Registering KT-1 to Cloudvue

Adding a multi channel camera to a Cloudvue Gateway

Description  This document will outline how to add a camera that has multiple channels but 1 IP address Product Cloudvue GatewaySteps to Reproduce  Notes If a master password is set this will be change the password when the first channel is added so the master password will need to be used for channels 2,3 & 4… Continue reading Adding a multi channel camera to a Cloudvue Gateway

Alarm Output Soft triggers on Thin Client triggering on and off automatically

DescriptionWhen a Alarm Output Soft Trigger is enabled in the thin client it triggers on and off every 10 seconds automatically. Product Exacq Thin Client Exacq Web Service Steps to Reproduce Setup an alarm output to a soft trigger on exacq Access this soft trigger on the thin client Enable the soft trigger Expected Results Alarm stays on… Continue reading Alarm Output Soft triggers on Thin Client triggering on and off automatically