Exacq AV1 Codec Support

Description Exacq are in the process of adding support for the AV1 Codec. AOMedia Video 1 (AV1) is an open, royalty-free video coding format initially designed for video transmissions over the Internet. It was developed as a successor to VP9 by the Alliance for Open Media (AOMedia),[2] a consortium founded in 2015 that includes semiconductor firms, video on demand providers, video content producers, software development companies and web browser… Continue reading Exacq AV1 Codec Support

Hikvision Camera losing motion / stops recording

Description This resolves the issue where the camera recording is stopped on motion recording schedule. The user then has to disable and re-enable the camera for it to start recording again. Product Exacq, Exacq Vision Client. Solution User has to upgrade to 22.12 or later.

No view on Cloudvue cameras – Buffering on full screen

Description This deals with the issue where C2C cameras on cloudvue are online but nothing shows on live view on cloudvue. When full screen is toggled on the cloudvue interface, the live feed starts buffering. Solution

Cloudvue Analytic Snapshot – Via Email

Description This is for the issue where snapshot analytics do not show up via email on Cloudvue. Explanation / Solution This is as designed on Cloudvue. This feature could be rolled out on later versions of cloudvue.

Understanding and Using Partner Codes

Understanding and Using Partner Codes Partner codes are the way in which Cloudvue can group devices (Cloud Cameras.and Cloudvue Gateways) under certain owners or a managers. Add a Partner Code to a Device Log into Cloudvue Enterprise Manager and find the selected device: Click on EDIT DEVICE and enter the partner code then click on… Continue reading Understanding and Using Partner Codes