Author: Lauren McTeague
Configuration Calculator
This tutorial video showcases the new metadata updates on the exacqVision Configuration Calculator.
Illustra Edge Analytics
This tutorial video showcases how to configure Illustra Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:40 exacqVision Client Configuration02:34 Search3:55 Event Linking
Hanwha Edge Analytics
This tutorial video showcases how to configure Hanwha Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:25 exacqVision Client Configuration02:10 Search3:12 Event Linking
Axis Edge Analytics
This tutorial video showcases how to configure Axis Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:22 exacqVision Client Configuration02:14 Search3:00 Event Linking
exacqVision 25H1 Release Bulletin
Persistent Event Monitoring in exacqVision Client 25H1
The Persistent Event Monitoring feature in exacqVision Client 25H1 allows users to ensure that event monitoring persists, even if the Client is closed, providing continuous surveillance and notifications of events. The Event monitoring feature in exacqVision has over many years provided a flexible way to bring in situation awareness for the live monitoring use case.… Continue reading Persistent Event Monitoring in exacqVision Client 25H1
Scheduled Exports in exacqVision Client 25H1
This feature included in exacqVision Client 25H1 allows the user streamline the video exporting process by exporting video footage at a scheduled time – for example overnight when the network traffic is minimal. exacqVision allows the user to export video for sharing from it’s search interface. The video from one or more cameras is downloaded… Continue reading Scheduled Exports in exacqVision Client 25H1
Edge Cloud Archiving in 25H1
Support has been added in exacqVision 25H1 for archiving to Amazon S3 or Wasabi target. exacqVision Edge brings the comprehensive capabilities of a VMS to a supported camera, enabling camera-only installs. exacqVision Edge solution avoids the need to have an NVR on premise that needs to be deployed and maintained. The video data was vulnerable… Continue reading Edge Cloud Archiving in 25H1
Configuring RTSP Streams in exacqVision Client
Note: This is an INTERNAL document – please do not share. VLC Configuration Add the RTSP Stream to exacqVision Client