Windows 10 Enterprise LTSB Not Able to Change Network to Private

Problem

For exacqVision systems running Windows 10 Enterprise LTSB, the network policy will default to “Public” if the only network connection does not have a Gateway, or is not attached to a Domain.

<br>

Cause

This is due to the Network Location Awareness not being able to identify the network.

<br>

Resolution

NOTE: This fix will permanently change all unidentified connections to “Private”.

1. Log in to the OS with a Admin level user.

2. Open the Command Prompt, selecting “Yes” on the UAC prompt, type the following command, then click “Enter”.

gpedit.msc

3. Navigate to: “Local Computer Policy > Computer Configuration > Windows Settings > Security Settings > Network List Manager Policies”

4. Double-click on “Unidentified Networks” and select “Private” under “Location type”.

5. Click “OK”, close the “Local Group Policy Editor” and Command Prompt.

<br>

Windows-10-Enterprise-LTSB-Not-Able-to-Change-Network-to-Private.pdf