ExacqVision Foreign Configuration Message

Title

ExacqVision Foreign Configuration Message

Description 

Meaning of Foreign Configuration message from RAID

Product 

ExacqVision Server

Information

Each drive in RAID Controller’s configuration has a bit of information about the controller it is on written to it. 
Sometimes, a RAID Controller will detect that information about a controller exists on one or more of the drives, but it does not match what the controller expects. 


Solution

If the customer has moved hard disks from one machine to another:

If the customer does not need the data from the newly inserted drives, the Foreign Configuration can be cleared, and the newly added drives can be imported into the RAID.

If the RAID Controller has been replaced:

The Foreign Configuration should be imported from the Drives into the RAID Controller.