Description
The exacqVisionOVID.deb file available at https://exacq.com/reseller/exacqVisionOVID.deb fails to install on both Ubuntu Linux 18.04 and 20.04.
Product
- S2 Integration
Steps to Reproduce
- Download https://exacq.com/reseller/exacqVisionOVID.deb
- Run the command
dpkg -i exacqVisionOVID.deb
Expected Results
The OVID package installs successfully
Actual Results
The install fails with the following error.

Solution
Run the following commands. NOTE: ./cfgedit still fails to work but caja can be used to edit ovid.ini
- sudo dpkg –add-architecture i386
- sudo apt update
- sudo apt install zlib1g
- sudo apt –fix-broken install
- sudo dpkg -i exacqVisionOVID.deb
- sudo ./cfgedit
- ./cfgedit: error while loading shared libraries: libz.so.1: cannot open shared object file: No such file or directory
- use caja instead to edit ovid.ini
- sudo caja
- navigate to /usr/local/exacq/ovid
- directly edit the ovid.ini file
See trac Ticket #23269 for additional details