Reboot or Default a Camera from the exacqVision Client

Description 

Prior to the release of exacqVision Client Version 22.03 cameras could not be rebooted or factory restored via the Client.  With the introduction of the Camera Web Configuration feature, cameras can now be rebooted or factory reset from within the Client.   

Product 

  • exacqVision Client

Solution

  • Access the cameras web interface via the camera web configuration page.
  • See Knowledge Base Article KB #7274  “exacqVision Camera Web Configuration Page” for instructions
  • Follow the camera manufacturers instructions to either reboot or factory restore the camera.

<br>