Description
In order to accommodate more than 4 channels of video, many multi-channel encoders require the use of the “bank” IP plugin override. The cameras test records should indicate this in the Notes.
Solution
- 1st bank channels 1-4, no override required
- 2nd bank channels 5-8, #bank=2
- 3rd bank channels 9-12, #bank=3
- 4th bank channels 13-16 #bank=4
For Example, assuming the cameras IP address is 192.168.1.1:
1st bank would be: | 192.168.1.1 |
2nd bank would be: | 192.168.1.1#bank=2 |
3rd bank would be: | 192.168.1.1#bank=3 |
4th bank would be: | 192.168.1.1#bank=4 |
<br>