Categories
Knowledge Support Support exacqVision Server

Samsung Trigger Inputs Not working

Description

When the input is triggered on the camera, the input trigger in exacqVision client does not change state.  
Note: this effects Samsung SUNAPI2 cameras

Steps to Reproduce

  • Connect a switch to the cameras input trigger. 
  • In the camera
    • Configure Alarm output 1 (N.O.)/Pulse/5s
  • In the Client
    • add the camera using the Samsung plugin
    • Configure Trigger Input (Open)
    • Verify trigger status Normal and Connection Status Connected
  • Trigger the switch connected to the camera

Expected Result

  • Trigger Input 1’s trigger status changes to alarm in the client.

Actual Result

  • Status does not change in the client

Work Around

  • None at this time, but there will be a fix available in exacqVision Server 22.03.