Categories Knowledge Support Support exacqVision Server Categories 2N devices will not detect motion Post author By Bhargav Atturu Post date January 5, 2022 I have seen this on two different devices, 2N Force IP and 2N Solo IP You will need perform the following steps Go in to the cameras Web GUI under Services Then click on Automation Click on Edit for Function1 -Under Events, drag the Event titled MotionDetected over to the drawing board on the right-Click on Events at the top of the list and pick an input from the next group.-Pick the one called SetOnvifVirtualInput and drag it over to the drawing board.-Set the State of the MotionDetected box to Start-Draw a connector line from Event to Event-Set the port to 1-Set Level to HiRepeat the process-Under Events, drag the Event titled MotionDetected over to the drawing board on the right-Click on Events at the top of the list and pick an input from the next group.-Pick the one called SetOnvifVirtualInput and drag it over to the drawing board.-Set the State of the MotionDetected box to End-Draw a connector line from Event to Event-Set the port to 1-Set Level to LoClick on SAVE in the top right cornerUnder Add IP Cameras, disable the device and Re-enable the deviceTest to see if it is detecting motion correctly now Tags Motion Detection Not Working, 2N Force, 2N Solo, 6685, Guest ← Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows → LSI Recommendations on Drive Capacity