Limited Features available in the Thin Client .

This is not an exhausted list.
Soft Triggers are not available in the Web Browser/Thin Client. Customers should use the Exacq Mobile 3 Client from a Web Browser instead.

The physical triggers are located in the menu of the mobile browser instead of on the live view.

For Example:
If you are using a trigger for audio and the associations have been created.
Connect to the Exacq Mobile 3 Client in a browser, navigate to the menu options, go to the Audio Devices, select Audio Input, and select Listen in Live.
In the lower right corner you will see the option for activating that soft trigger.