Categories
Knowledge Support Support exacqVision Server Categories Products

The IP Camera Detect Plugin Doesn’t Load on Server v20.06.4 if Installed on Ubuntu 18.04 Systems

The IP camera detect plugin does not load on server software version 20.06.4 if installed on servers with the Ubuntu 18.04 operating system.

Issue:

The IP camera detect plugin does not load on server software version 20.06.4 if installed on servers with the Ubuntu 18.04 operating system.

Description:

On the server software 20.06.4/18.04 OS combination, IPCamDetectPI fails to load, and in turn, IP camera detection is not available in the exacqVision Client interface. The “Add IP Cameras” page does not display the “Find IP Cameras” and “Address IP Cameras” tabs on the bottom half of the page.

Logs show the following:

Core     Critical     Core: Failed to load plugin 'IPCamDetectPI.so': /usr/local/exacq/server/plugins/IPCamDetectPI.so: undefined symbol: _ZTIN7testing4TestE

Introduced In:

Version 20.06.4

Fixed In:

Version 20.06.5+