Retail Key Image Release Highlights – 202108

August 27,2021

New and updated zip files are now available on the public website

https://www.exacq.com/support/downloads/
Username: guest 
Password: exacqvisionip

 Highlights:

  • Introduced Ubuntu 20.04 (18.04 is now deprecated
  • Updated field recovery instructions are packaged within the zip files
  • The following motherboards do NOT support Ubuntu 20.04 and servers with these motherboards that need to be re-imaged must use Ubuntu 18.04/RETAIL1804-21.03.5.zip
    • Q87MA
    • H81-X1
    • D180S
    • D190S
    • D290S
  • Customers who only have LTSB license must use Windows 10 LTSB/RETAIL10-20.03.0.zip
  • Customers who only have 2016 license must use Windows Server 2016/RETAIL2016-20.06.0.zip
  • Transition from grub to rEFInd (look and feel has changed as noted in field recovery instructions).
  • Transition from custom-built Clonezilla to off-the-shelf Clonezilla which adds progress bars, much nicer.
  • Automatic recovery partition creation, once Deploy Cleanup (desktop shortcut) is executed, the system will automatically reboot and capture factory image, then automatically reboot again into OOBE.
  • New error log, if any errors occur anywhere in the entire process, there will be a collection of logfiles written to the “logs” folder on the USB key itself.  Users can provide these to us for analysis.