Storage Hardware Attribute Alarms from 3rd Party HDDs

Servers are reporting Health Warnings in exacqVision Enterprise Manager.  The event details in EM show “This result is based on an Attribute check on Disk /dev/csmi0,2” 
Note: the device may vary for example /dev/csmi0,0 instead of csmi0,2 or perhaps both.

The corresponding exacqVision Enterprise Manager logs show:

5/9/2021 02:09:11.356 PM  (GMT-7:00)     SysMgmtPI     Warning                     5516# Disk = /dev/csmi0,2 Status = This result is based on an Attribute check. 

It has been determined that these are false positives and can safely be ignored as they do not affect normal operations.  A fix will be available in exacqVision Server 21.09.