Axis Camera Q3515 Auto Focus Button doesn’t show up in Client

If the client does not show the Auto Focus Button in the clients camera setting page please do the following.

This can be seen on server/client 19.12 through 21.06. This is a camera side issue and not server related.

Axis sent instructions to tech for case 02148631.

  1. Default the Camera via gui. Make sure the camera is not connected to our client.
  2. Update the FW of the camera to latest of Axis website. FW10.6.0
  3. Then connect the camera to the server.