How do I find my hostname for Exacq Cloud-Integrated Service Portal

Someone asks, “What is my FQDN, Hostname or IP Address I need to put in to my Firewall for Exacq Cloud-Integrated Services Portal to work correctly?”

It is the customers URL they access for the Integrated Services Portal https://exa001.exacq.net the part in BOLD is specific to them and starts with three letters and followed by three numbers. It uses port 35111 for outbound connections.

Configuring outbound connections

About this task

To configure an outbound connection, connect the exacqVision client to the server. On the Outbound Connections tab, you can connect to services outside the system’s network, such as exacqVision Enterprise Manager or exacqVision Integrator Services Portal. Using an outbound connection, it is not necessary to configure inbound firewall rules for exacqVision Enterprise Manager to reach the server. Ensure that the server has outbound access on port 35111.

Procedure

To configure an outbound connection, complete the following steps:

  1. In the Configuration pane, click System Configuration.
  2. Click the Outbound Connections tab.
  3. In the exacqVision Enterprise Manager configuration pane, click Configure.
  4. From the Server Account list, select an Admin user configured on the server for exacqVision Enterprise Manager to use.
  5. Enter the email address, and password of your exacqVision Enterprise Manager dealer account.
  6. Click OK.

Results

If the exacqVision server can reach exacqVision Enterprise Manager, the URL of the exacqVision Enterprise Manager dealer instance populates in the outbound connections list.