Panasonic cameras OSD incorrect after Server time change

Issue:

After a Server time change of less that 60 seconds, Panasonic cameras may continue to show the OSD time incorrectly until the camera is disconnected/reconnected.

The stored video also contains the incorrect time-stamp. This means the searched video will be off by the amount of seconds that they system time changed.

Workaround:

Disconnect and reconnect the camera on the Add IP Cameras page.

Fixed In:

Dev 21.06.108
Expected in public release 21.09.