Categories
Video Library Demo exacqVision Enterprise exacqVision Client exacqVision Server exacqVision Mobile Categories exacqVision Webservice exacqVision Hardware Products

2020-06-11 – June Quarterly Release Training

Client

  • Enhancement – Support for custom categories and confidence levels. #21037
  • Enhancement – Add link to Facial Matching in the Automations Engines panel.
  • Enhancement – Add Unmerge command in Facial Matching panel.
  • Enhancement – Support GPU decoding with multiple GPUs. #17520
    https://trac.exacq.com/DVR/wiki/HardwareDecoding#MultipleGPUDecoding
  • Enhancement – Several improvements to performance of copy-back rendering from a GPU decoder.
  • Enhancement – Improve performance of GPU decoding in conjunction with dewarping.
  • Enhancement – Minor performance improvements to rendering and colorspace conversion.
  • Enhancement – Improve GPU decoding calibration performance estimates.
  • Enhancement – Improved handling of exacqReplay when Search Permissions are disabled #20931
  • Enhancement – Replaced wodim burning software with evburn on Windows and libburn on Linux #8585
  • Bug Fix – Delete cached config files when deleting server #20877
  • Bug Fix – If a user on an offline searchable system and gets disabled, disallow any further offline searching. #21161

Server

  • Enhancement – tycodlpi – Support user-configurable classifications. #20998
  • Enhancement – NetworkStoragePI – Add OS-on-RAID support, fix partitioning of small RAID volumes. #21083
  • Enhancement – StreamPI – Support network configuration for GPoE 16-port model. #21130
  • Enhancement – SysmgmtPI – Improve graphical storage layout GUI for OS-on-RAID zero-drive models. #21158
  • Enhancement – SysmgmtPI – Allow drive prep for restricted BBE systems (LC-Series and G-Series).
  • Bug Fix – SysmgmtPI – Fix drive prep of multiple disks to prevent accidentally giving same mount point to multiple disks. #20226
  • Enhancement – core – Added debug logging of memory and queue stats. #21156
  • Enhancement – Illustr3PI – Support temperature alarms. #21121

Web Service

  • Feature – I-frame only mode for video endpoints. #20995
  • Enhancement – Allow transcoding parameters to be updated during a websocket video stream. #21122
  • Bug Fix – Allow loading of images for Tyco Cloud.

Mobile

  • Feature – Add configuration of camera OSD settings. #20722
  • Enhancement – Support additional OSD style settings. #20722
  • Enhancement – Added ability to modify camera names.
  • Enhancement – Enabled cloud archive search in browser environments.
  • Enhancement – Stream motion JPEG video over websockets where applicable. #20994
    – Mostly impacts iOS.
  • Enhancement – Added camera preview video to camera settings page. #15727
  • Enhancement – Camera details option on video context menu. #20725
  • Enhancement – Prefer most likely to connect network address on startup. #18971
    – First attempt will be to connect to the most recently used connection type.
    – Then additional connections will be made in the background and will ‘upgrade’ seamlessly.
    – The full connection order is as follows:
    •   original (if https and not relay)
    •   internal (https)
    •   external (if https)
    •   detected (https)
    •   original (if http)
    •   internal (http)
    •   relay (relay is always https)
    •   external (if http)
    •   detected (http)
  • Bug Fix – Removed support for web service versions 7.4 and below. #20610

Enterprise Manager

  • Feature – Support for system backup and restore #19149
  • Enhancement – Improved failover processing #19990