Skip to the content
Server
- Enhancement – core, LogPI – allow to dynamically control logging level per plugin #19954
- Enhancement – itv2pi – Add more verbose logging and debug logging to help troubleshoot issues in the field
- Enhancement – streampi – Adding logging to help troubleshoot LDAP binding issues
- Enhancement – rtspserverpi – plugin to provide rtsp stream from server. #19100
- Feature – First Illustra Edge Pro Gen3 server release. #18275
- Enhancement – onvifnvcpi – Uniview alias in json. #20099
- Enhancement – hikvisionpi – add Grundig OEM. #19944
- Enhancement – hikvisionpi – support analytics events. #6118
- Enhancement – onvifnvcpi – support backoff retry connection logic. #19240
- Bug fix – IllustraStandardIN – default to local camera timezone setting. #19911
- Enhancement – onvifnvcpi – Dahua multi-sensor motion support and analytic in json.
- Bug Fix – onvifnvcpi – support motion event for SightLogic multi-sensor. #19819
- Enhancement – onvifnvcpi – support motion/input trigger events for Avigilon multi-sensor. #19966
- Enhancement – SysmgmtPI – Eliminate hwmconfig entries for temperature for non-RAID systems, and generalize rules for RAID systems to minimize updates. #14914
- Enhancement – SysmgmtPI – Add blacklist for disk models that don’t support standardized temperature SMART attributes, to prevent false storage alarms. #19497
- Bug Fix – SysmgmtPI – Use raw value for SMART temperature attribute 194 (defined as actual celcius value) instead of manufacturer-specific normalized value, which can cause false-positive storage alarms. #19685
Client
- Enhancement – Added support for webhooks #19304
- Enhancement – Allow changing of IP camera plugin on local server. #18572
- Enhancement – Added startup instance count to client settings. #20304
- Bug Fix – macOS – Resolved several display issues on Mojave and Catalina. #18886
- Bug Fix – macOS – If install path is not writable possibly due to translocation then install to the default path of Applications instead. #19901
- Enhancement – Securely pass EM sync credentials to exacqReplay to avoid re-prompts. #19295
- Enhancement – Securely pass second reviewer credentials to exacqReplay to avoid re-prompts. #19295
- Enhancement – Added client dewarping support for Axis M3067 and M3068. #20280
- Enhancement – Debug Log level option now available for configuration per plugin #19701
- Enhancement – Stream properties accessible when toolbars are hidden. #18513
- Enhancement – Provide a quick link from camera configuration to associations configuration. #20125
- Enhancement – Added support for drag and drop Views/Tours/Event Monitor Profiles operations. #18817
- Enhancement – Move cursor to the start of the bookmark time on search. #19913
- Enhancement – Upgraded wxWidgets version. #17978
- Enhancement – Added translations for Chinese (Taiwan) locale.
Web Service
- Enhancement – Remove default admin account on new deployments. #20245
Mobile
- Feature – Refactored focus page to increase usability. #19494
- Feature – Replaced action menu with client-style associations bar, following associations configuration. #19502
- Feature – Camera details page with basic camera information. #19501
- Enhancement – Performance improvements during startup and server connection.
Enterprise Manager
- Feature – Channel pool that allows users to transfer unused channels to servers #18682
- Enhancement – Migrate server/camera event detail pages to React #19514
- Enhancement – Better license conflict warning messages #20027
- Enhancement – Add utils to save and apply a backup #18521
- Enhancement – Allow setting default admin credentials with administrator access #19331
- Enhancement – Update to ODBC Driver 2017 for SQL Server #19678
Image
- Linux 18.04 Out of Box Experience (OOBE)