Client
- Enhancement – Added RTSP server configuration page. ›Still requires
– Server-side work. - Enhancement – Added AutoGroups to automatically populate groups based on attributes assigned for cameras and/or systems. – #18433
- Enhancement – Advanced filtering for camera and system metadata
- Enhancement – Password fields no longer auto populate.
- Enhancement – Added support for dynamic camera plugin settings
- Enhancement – Added support for dynamic camera plugin settings
– “Advanced” tab - Enhancement – Acti B78 model added to Dewarp library
- Enhancement – Enable GPU decoding on 18.04 LC systems.
- Enhancement – macOS – Add support for 10.15 and drop support for 10.8 and below.
- Bug Fix – Include syslogs in support export by default on local systems.
- Bug Fix – Allow microphone when no speakers are connected – #19027
Server
- Enhancement – pospi – support pos database encryption
- Enhancement – illustra3 – support exposure profile configuration.
- Enhancement – Onvif – updated motion/input trigger support for GeoVision.
- Enhancement – kantechpi – enhanced activity logging to aid troubleshooting – #19159
- Enhancement – Illustra3, Onvif, ACTi – Improve initial RTSP connection speed. – #18860
- Enhancement – dahuaippi – support timestamp with server option.
– https://trac.exacq.com/DVR/wiki/IpPluginOverrideOptions - Enhancement – PTZPI – AD-MP3200 / AD-MP48 multi prioritize recent PTZ commands when selecting determining which terminator to use.
- Enhancement – PTZPI – AD-MP3200 / AD-MP48 multi don’t send monitor and camera callups with no additional commands.
- Enhancement – PTZPI – AD-MP3200 and AD-MP48 added support for patterns.
- Enhancement – PTZPI – AD-MP3200 and AD-MP48 added support for flip and apple peel commands.
- Enhancement – PTZPI – AD-MP3200 and AD-MP48 added support for auto iris / focus.
- Enhancement – PTZPI – AD-MP3200 and AD-MP48 Multi prevent utilize multiple devices per port when sending PTZ commands and avoid monitor selection overhead with every command.
Web Service
- Feature – Support for analytics push notifications.
- Enhancement – Reduce push notification throttle for triggers from the same source to 30 seconds.
- Enhancement – Add interface to configure HTTP policy. – #15461
Mobile
- Feature – Push notifications for analytic rules
- Enhancement – Improve speed of network address selection when initializing a web service. – #18999
- Enhancement – Removed Event Profile Dialogs, replaced with Event Profile Page
Enterprise Manager
- Feature – Synchronize server licenses with license server – #18684
- Enhancement – Updated Enterprise Manager header bar – #18351
- Enhancement – Added section to download EM log files from EM header info about section, for root admin users
- Enhancement – Migrated to python 3
– Downgrades are now broken without workarounds.
– https://trac.exacq.com/Support/ticket/3628