Affected platforms
exacqVision 7.4
<br>
Description
When integrating to a Neo panel using UDP configuration, in the exacqVision Client a UDP port number must be specified. Using the panel’s default will work for the first panel configured for that server. For all subsequent panels, first change the application UDP port number in the panel to some unique value, then specify this value in the exacqVision Client when configuring that connection.