Dewarping of Dahua cameras not working on web client or Exacq Mobile 3 (Legacy)

Affected Versions

  • exacqVision Web Service 7.6, running on Windows

<br>

Description

In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app.

<br>

Workaround

  1. Install the exacqVision Client on the web service or refer to an existing client installation on another machine.
  2. Copy C:\Program Files (x86)\exacqVision\Client\fish_eye.dll where the client is installed to the C:\Program Files (x86)\exacqVision\WebService\bin directory where the web service is installed.
  3. Restart the web service.

<br>

Resolution

Update exacqVision Web Service to version 8.2.2 or higher

<br>