iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution

Description

iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution

<br>

Summary

iOS Application crashes when decoding H.264 video from some axis sources in 800×450 resolution. This has been seen on a customers M5014 with firmware 5.25.2 as well as an M5014 with firmware 5.40.11.2 at the Exacq Fishers office.

<br>

Tested Version

Exacq Mobile 3, version 7.8.0

<br>

Platform

iOS

<br>

Steps to reproduce

  1. Connect to a web service that has an Axis M5014 camera that is streaming h.264 video in an 800×450 resolution.
  2. Add the camera to a 1×1 layout in an iPad

<br>

Expected result

Video is shown

<br>

Actual result

Application crashes

<br>

Work Around

Pick One:

  • Change the camera resolution
  • Change the image quality in the mobile application to be less than 70% of the image quality of the camera
  • View the camera on the mobile application in a video panel that is less than 45% or the height or width of the camera stream.