Pelco plugin with Optera crashes server

Description

Pelco plugin with Optera crashes server. ExacqRtsp_lib getSdpValue function is used by Pelco Optera to get the dewarp information with the RTSP session. The camera fails to return sdp and the default return of the getSdpValue method is NULL in this case.

Line 1148 ExacqRTSPCommandHandler.cpp.

<br>

Tested Version

  • exacqVision Server 7.9.39.102385

<br>

Steps to reproduce

  1. Connect to Pelco Optera (00-04-7d-0d-e8-54)
  2. When this happened, the camera was connected to another server(not sure is the cause)

<br>

Expected result

Server should not crash

<br>

Actual result

Server crashes

<br>