Samsung SUNAPI2 only handle the first input trigger event on a multiple digital input camera

Description

With newer Samsung models that supports SUNAPI2. Only the first input trigger is activated for cameras that have multiple trigger inputs.

<br>

Version Introduced

  • exacqVision Server 8.0.0.102418

<br>

Platform

All platforms for IP Cameras using Samsung plugin

<br>

Steps to reproduce

  1. Tested with SNP-L5233(00-09-18-41-34-F1 10.16.12.199) set with 4 input triggers
  2. Activate input triggers 2-4

<br>

Expected result

  • Input triggers 1-4 correctly alarmed
  • Event linking with each input trigger works as expected

<br>

Actual result

  • Input triggers 2-4 are not alarmed

Work Around

  • None

<br>

Version Fixed

exacqVision Server 8.1.4.102781

<br>