Missing ePlayer shortcut on Linux

Description

The ePlayer shortcut is missing from the menu. The player is still there and can be launched from the command line

<br>

Version Introduced

7.9.20

<br>

Platform

Linux

<br>

Steps to reproduce

  • Install client deb

<br>

Expected result

  • ePlayer shortcut under Exacq menu

<br>

Actual result

  • Only client shortcut under Exacq manu

<br>

Work Around

  1. Run ePlayer from commandline
  2. Downgrade to 7.8
  3. Run sudo xdg-desktop-menu install /usr/local/exacq/client/share/exacq-progs.directory /usr/local/exacq/client/share/exacq-player.desktop

<br>

Version Fixed

8.0.3 (when it comes out)

<br>

Keywords

eplayer, e-player, shortcut