Categories
Knowledge Support Support exacqVision Server Categories Products

Onvif with incorrect profile parameter in host name would crash server

Description

Onvif plugin does allow additional parameters in the host name for added supports. Such as profile/tranport settings(#Profile=1 or #transport=udp). Profile expects a number but would crash the server if a string is entered.

<br>

Version Introduced

r38461

<br>

Platform

All

<br>

Steps to reproduce

connect onvif camera with host name and profile with string.

example: 10.16.1.1#profile=test

<br>

Expected result

string in profile is ignored and defaulted to the first profile.

server does not crash.

<br>

Actual result

server crashes with invalid string entry.

<br>

Work Around

remove profile entry or reconnect with valid profile number.

<br>

Version Fixed

r103382 dev build 8.1.8.103450

<br>

Keywords

Onvif