USBDIO and Serial Port Recovery

The following recovery enhancements have been added to exacqVision Server:

  1. USBDIO recovery enhancement: version 6.7.20.74529
  2. UART serial ports recovery: version 6.7.25.75004

<br>

When a USBDIO or UART serial port device disconnects, exacqVision Server attempts to reconnect to the device after one second. If that attempt fails, the next attempt occurs after two seconds, and then four seconds, eight seconds, 16 seconds, and so on. This occurs until the device reconnects, or until the following maximum intervals are reached:

  1. USBDIO: 300 seconds
  2. UART serial ports: the same as the IP Camera reconnection interval