Samsung SNB-3002 Camera Allows Only Motion Non-detection Areas

Symptom

Samsung SNB-3002 cameras allow you to define non-detection motion areas. This is the opposite of most Samsung cameras, which allow you to define detection areas. There is no indication in exacqVision Client that an SNB-3002 camera motion window defines non-detection areas.

<br>

Workaround

When using exaqVision Client to configure a motion area for an SNB-3002 camera, define the area in which you want to ignore motion.