tDVR board fails to initialize after cold starting a system

Symptom

When starting a system from power-off the tDVR board fails to initialize, causing one or more of the following symptoms:

  • Blinking red LED lights near the processor.
  • Device Manager misreporting an 8008, 8016, or half of an 8032 as hardware ID 8000 in the Device Properties detailt tab.
  • Ispci not listing an Exacq Technologies 8008, 8016, 8032 device at all.

<br>

Affected platforms

All exacqVision systems with tDVR boards using tDVR Hybrid version < 1.2.20

<br>

Workaround

Power the system off, let it sit for 60 seconds or more. Power on the system again.

<br>

Resolution

Install tDVR Hybrid Driver 1.2.20 or greater and update the tDVR board bootloader.

<br>

Instructions:

For Windows:

  1. Download tDVR Hybrid Driver 1.2.20 exe file.
  2. Stop the exacqVision server in the Windows Service Control Manager
  3. Open the Command Prompt and Run “C:\Program Files\tdvr\board_info” -U
  4. View the output to verify that the bootloader was updated to version 1.1.1.665 or greater

<br>

For Linux:

  1. Download tDVR Hybrid Driver 1.2.20 deb file.
  2. Open a terminal session and stop the exacqVision server: sudo service edvrserver stop:
  3. Install the tDVR Setup version 1.2.20 sudo dpkg -i tdvr.deb
  4. Run the bootloader update command: /usr/local/tdvr/board_info -U
  5. View the output to verify that the bootloader was updated to version 1.1.1.665 or greater.
  6. Start the exacqVision server: sudo service edvrserver start