Affected platforms
exacqVision 4.10 to 7.0 (E-Series support introduced in 6.4)
<br>
Symptom
When attempting to add the 53rd E-Series encoder to a server, the 53rd E-Series will not connect. On Linux platforms the server will crash.
<br>
Workaround
If no Arecont, Illustra or UDP devices are being used on that server, install exacqVision development build 7.1.3402.84249. During the installation, uncheck the Arecont, illustra3 and UDP plugins at the “Select Components to Install” step.
<br>
Resolution
Fix expected in exacqVision 7.2