Axis HTTPS setup

To setup an Axis camera for HTTPS support in 8.4.1 server.

  1. Log into the camera web page and go to the setup page.
  2. Select “System options” and HTTPS.
  3. The HTTPS settings page might look different between fw’s.
  4. To create self signed certificates, select the create option and fill in the required fields such as country/locality/state/organization/etc in the popup.
  5. To load a certificate, select the install signed certificates option and navigate to the certificate.
  6. Install the certificate.
  7. Set the policy for admin/operator/viewer to https or both(http/https)
  8. The plugin will try https and if failed will then try http.
  9. The Client will show a lock beside the device to indicate HTTPS connections.