Using Soft Triggers from CCure 9000 with Event Linking

From the C-Cure 9000 interface, find the Camera ID as pictured below.

Setup a “Soft Trigger” under the “Action” tab.

Change the “Action Type” to “Soft Trigger.

Back in the exacqVision Client, create a new Event Link using the Event Type of “Soft Trigger” and the “Event Source” will match the Camera ID from above.