Camera discovery plugin leaks memory

Affected platforms

exacqVision 6.4 or higher

<br>

Symptom

Every time there is a config or alarm event from core, the IP camera detect plugin (IPCamDetectPI.dll) will leak memory. The memory leak is in small increments and on systems where huge number of events are happening, like lots and lots of motion events for example, the leak can grow to a few megabytes per day.

<br>

Work Around

No single work around that covers all cases. On certain cases like Onvif, minimizing the motion events by removing the json file entry to prevent motion events can mitigate the issue a lot.

<br>

Resolution

None at this time